STM32CubeMX bug for FDCAN?
Hi ST
I am using STM32CubeMX v6.10.0 with selected MCU STM32H563ZITx.
When configuring FDCAN1 I may have found a bug in the tool. The below two Nominal Time Seg1 and Seg2 say that the lowest value is "2" and the tool is limiting setting it to "1" which I think is a valid setting.


The RM0481 Rev 1 says that the minimum value that is interpreted by the hardware of that value is "1" (when register segment is set to "0")

Can someone please verify my findings?
Br
Imre