Skip to main content
ebrombaugh1
Associate III
December 26, 2025
Solved

STM32CubeMX fails to generate STM32H7RS PLL_USBPHYC initialization code.

  • December 26, 2025
  • 4 replies
  • 974 views

The STM32H7RS series includes a USB HS PHY with a special PLL that generates the 480MHz clock required as well as a 60MHz clock for the OTG HS peripheral and optionally a 48MHz clock for the separate OTG FS peripheral. The PLL for the USB PHY has several configuration bitfields in the RCC->CCIPR1 register that are used to set the source of the PLL reference clock, as well as its frequency:

 

Bits 13:12 USBPHYCSEL[1:0]: USBPHYC kernel clock source selection. Set and reset by software.
00: hse_ker_ck (default after reset)
01: hse_ker_ck / 2
10: pll3_q_ck
11: reserved, the kernel clock is disabled


Bits 11:8 USBREFCKSEL[3:0]: USBPHYC kernel clock frequency selection .Set and reset by software.
This field is used to indicate to the USBPHYC, the frequency of the reference kernel clock provided
to the USBPHYC.
0011: The kernel clock frequency provided to the USBPHYC is 16 MHz
1000: The kernel clock frequency provided to the USBPHYC is 19.2 MHz
1001: The kernel clock frequency provided to the USBPHYC is 20MHz
1010: The kernel clock frequency provided to the USBPHYC is 24 MHz (default after reset)
1110: The kernel clock frequency provided to the USBPHYC is 26 MHz
1011: The kernel clock frequency provided to the USBPHYC is 32 MHz

Within the STM32CubeMX GUI the USBPHYCSEL bits are controlled by a mux selection on the clock configuration tab and the USBREFCKSEL bits are determined by a drop-down menu in the USB OTG HS configuration menu. When generating source code the USBPHYCSEL setting is reflected in the HAL_PCD_MspInit() function, properly setting the PeriphClkInit.UsbPhycClockSelection value.

The problem is that the USBREFCKSEL bits are never changed from the default 24MHz setting even if the drop-down menu in the CubeMX GUI has been correctly set. There is a function for setting them - LL_RCC_SetUSBREFClockSource(uint32_t ClkSource) but it is never called from within either HAL RCC or from within the generated source.

Ideally STM32CubeMX would generate a call to LL_RCC_SetUSBREFClockSource() with the proper argument based on the user setting in the GUI (and the clock configuration tab would include appropriate error checking on this value), or else some warning commentary that the user is responsible for handling this themselves.

Best answer by FBL

Hi @ebrombaugh1 

The second issue you reported is already addressed here: Solved: STM32CubeMX H7S3 RCC_CCIPR1 incorrect initalization

4 replies

TDK
Super User
December 27, 2025

Include the IOC you're having issues with.

Works fine here. In initialization code:

TDK_0-1766798580917.png

Actual bits get set here:

TDK_1-1766798710678.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
ebrombaugh1
Associate III
December 29, 2025

Thanks. Digging into stm32h7rsxx_hal_rcc_ex.h you can see that function is not actually touching the bits which tell the PLL what the reference frequency is.

ebrombaugh1_0-1767042768185.png

That function only controls the input mux setting via the USBPHYCSEL bits, choosing the PLL3Q input in this case. It does not select the frequency controlled by the USBREFCKSEL bits.

So I've closed this issue prematurely - too bad that one can't undo that as this is not solved.

 

Technical Moderator
December 29, 2025

Hello @ebrombaugh1 

This article may help you as well FAQ: Troubleshooting a USB core soft reset stuck.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
TDK
Super User
December 29, 2025

You can unmark a solution.

Again, please include the IOC file you are having trouble with so the issue can be replicated.

"If you feel a post has answered your question, please click ""Accept as Solution""."
FBLBest answer
Technical Moderator
December 30, 2025

Hi @ebrombaugh1 

The second issue you reported is already addressed here: Solved: STM32CubeMX H7S3 RCC_CCIPR1 incorrect initalization

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
ebrombaugh1
Associate III
December 31, 2025

Thanks - that appears to address the issue, and from what I see there is a workaround for the current HAL release and the team is aware and working to correct it in a future release.