Skip to main content
Best answer by Ghofrane GSOURI

Hello @ElectronicABC 

This is not blocking: it’s just a warning, not an error, so you can press “Yes” and the code will still be generated.

The warning simply indicates that there may be a logical/configuration issue in the LPBAM setup, even though valid C code is produced.

If the example runs correctly on your board, you can safely ignore the warning.

If the behavior is not as expected, use this warning as a clue to review the LPTIM and LPGPIO settings in the LPGPIO_drive LPBAM application.

THX

Ghofrane

2 replies

Associate II
January 25, 2026

ElectronicABC_0-1769325942127.png

 

 

Associate II
January 25, 2026

 

click check ,only show this 

ElectronicABC_2-1769326034636.png

 

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
January 26, 2026

Hello @ElectronicABC 

This is not blocking: it’s just a warning, not an error, so you can press “Yes” and the code will still be generated.

The warning simply indicates that there may be a logical/configuration issue in the LPBAM setup, even though valid C code is produced.

If the example runs correctly on your board, you can safely ignore the warning.

If the behavior is not as expected, use this warning as a clue to review the LPTIM and LPGPIO settings in the LPGPIO_drive LPBAM application.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.