STM32CubeMX Pin Re-assignment on STM32U5A9 - Questions
Hello Forum,
I've noticed a feature/bug/behaviour in CubeMX 6.15.0 that I'm unsure about so could do with some advice. I've been configuring an STM32U5A9ZJT 144 pin MCU for a project I'm working on. This has been an evolutionary process. To make the point I'll just focus on two peripherals, LPUART1 which has already been configured and I2C3 that I want to add in and configure.
I start with LPUART1 configured as follows:

Which has pins assigned like this on the MCU:

I then enable the previously disabled I2C3 peripheral - there's nothing to say it conflicts with anything. This results in I2C3 looking like:

Having done this CubeMX silently reconfigured the LPUART1 pins.

thus:

So the question is: "Is this normal?" If so I've never noticed before. It seems odd to me as I could have had a physical board made with the LPUART1 pins setup in the initial config. Adding the I2C3 peripheral breaks LPUART1.
Any thoughts/advice much appreciated.
DD