Skip to main content
Kneepatch
Senior
December 18, 2024
Solved

STM32F469I-DISCO Missing fatfs.h after using CubeMX to Generate Code

  • December 18, 2024
  • 2 replies
  • 1173 views

I'm missing the FATFS supporting library files after adding SDIO SD card support and FATFS support in the CubeMX code generation tool within STM32CubeIDE.

Kneepatch_1-1734490372665.png

 

Kneepatch_0-1734490318906.png

The funny thing is that those files are present in the project folder, just not in my project's folder structure in STM32CubeIDE.

Kneepatch_2-1734490434741.png

What I am doing wrong here? I was under the impression that the CubeMX tool was supposed to add/link these files to the project automatically.

 

Best answer by Kneepatch

@Andrew Neil wrote:

If they are there, does it work if you add them to the CubeIDE project?

(yes, that does still leave the question of why CubeIDE didn't include them properly)

 


Funny enough, if you do add all of the various files it complains about into a single folder, it is happy. Here is what I ended up doing:

 

Kneepatch_1-1736334489505.png

Now I don't get any errors. Mystery is still why CubeMX isn't able to add these to my project when I generate the code.

2 replies

Technical Moderator
December 18, 2024

Hello @Kneepatch 

Thank you for posting!

Are you using the latest version of CubeMX 6.13.0.

KR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Kneepatch
KneepatchAuthor
Senior
December 19, 2024

Hey @Souhaib MAZHOUD, I am using the latest CubeMX 6.13.0 software:

Kneepatch_6-1734578430945.png

 

-Kneepatch
Andrew Neil
Super User
December 18, 2024

@Kneepatch wrote:

The funny thing is that those files are present in the project folder, just not in my project's folder structure in STM32CubeIDE.


Not quite sure what you mean by that - please show the project structure.

Windows explorer folder tree view would also be useful.

If they are there, does it work if you add them to the CubeIDE project?

(yes, that does still leave the question of why CubeIDE didn't include them properly)

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Kneepatch
KneepatchAuthor
Senior
December 19, 2024

Here is the project structure:

Kneepatch_0-1734577316309.png

Windows Explorer:

Kneepatch_2-1734577785154.png

I have tried linking them in the project manually like this, it just ends up breaking references in a different way. It makes me feel like this problem is a deep rabbit hole. I try to mimic to the best of my ability the same structure that is in Windows Explorer, even though it's not exactly one for one. Here is my attempt at linking them manually and the errors that I get:

Kneepatch_3-1734577868423.png

Kneepatch_4-1734578169508.png

Kneepatch_5-1734578206363.png

 

 

-Kneepatch