STM32H5: CubeMX generates USBX device stack init function but never calls it
I found what looks like a reproducible STM32CubeMX code generation bug for STM32H5 USBX device projects.
I tested this on a fresh project, so this does not appear to be a migration issue from an older codebase.
Problem
CubeMX generates these USBX init functions:
- MX_USBX_Init()
- MX_USBX_Device_Init()
- MX_USBX_Device_Stack_Init()
However, the generated call flow only invokes:
- MX_USBX_Init()
- MX_USBX_Device_Init()
and never calls MX_USBX_Device_Stack_Init().
That is a problem because MX_USBX_Device_Stack_Init() contains the actual device stack setup:
- ux_device_stack_initialize(...)
- class registration
- ux_dcd_stm32_initialize(...)
Without that function running, the USB peripheral can start and receive a reset interrupt, but USBX has not been given valid device framework pointers yet.
Observed failure
When USB_DRD_FS_IRQHandler() fires and the USB reset path runs, the code eventually reaches:
- HAL_PCD_ResetCallback()
- _ux_dcd_stm32_initialize_complete()
- _ux_utility_descriptor_parse(...)
and hard faults inside _ux_utility_descriptor_parse, because the device framework pointer was never initialized.
In my case the hard fault occurred at the byte dereference in _ux_utility_descriptor_parse().
Generated code pattern
MX_USBX_Init() does:
- ux_system_initialize(...)
- MX_USBX_Device_Init(...)
but does not call MX_USBX_Device_Stack_Init().
MX_USBX_Device_Stack_Init() is generated correctly, but left unused.
Expected behavior
The generated code should call MX_USBX_Device_Stack_Init() after ux_system_initialize(...) and before MX_USBX_Device_Init(...), so the order is effectively:
- ux_system_initialize(...)
- MX_USBX_Device_Stack_Init()
- MX_USBX_Device_Init(...)
- USB thread configures PMA and starts PCD
Workaround
Manually add the missing call so that MX_USBX_Init() does:
if (ux_system_initialize(pointer, USBX_MEMORY_STACK_SIZE, UX_NULL, 0) != UX_SUCCESS)
{
return UX_ERROR;
}
if (MX_USBX_Device_Stack_Init() != UX_SUCCESS)
{
return UX_ERROR;
}
if (MX_USBX_Device_Init(byte_pool) != UX_SUCCESS)
{
while(1)
{
}
}Why I believe this is a CubeMX bug
I reproduced this with a brand-new test project generated from scratch, not just an upgraded older project.
Has anyone else seen this on STM32H5 + Azure RTOS USBX device projects, and can ST confirm whether this is a known generator issue?
If needed, I can also post the exact generated files showing the missing call path.