STM32H563 using CUBEMX and LL - UART9 does not have its Baud Rate Register initialized correctly
I'm using a STM32H563 Nucleo and the latest version of CubeMX along with the Keil (V6.19 C Compiler - uVision IDE V5.38)
I have discovered a weird issue where even though CubeMX seems to be generating the initialization code for the baud rate for UART9 correctly, it does not actually get loaded into the UART9 Baud Rate Register (BRR) using the Lower Level (LL) libraries:
UART_InitStruct.BaudRate = 19200;
UART_InitStruct.DataWidth = LL_USART_DATAWIDTH_9B;
UART_InitStruct.StopBits = LL_USART_STOPBITS_1;
UART_InitStruct.Parity = LL_USART_PARITY_ODD;
UART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
UART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
UART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(UART9, &UART_InitStruct);
LL_USART_ConfigAsyncMode(UART9);
LL_USART_Enable(UART9);
When I compile and execute the code, the USART_BRR value stays unchanged at 0 hex. I have tried the same thing on UART7 and it works just fine. I am trying to trace through the LL code and see where it's failing to load the UART9 BRR, but in the meantime I thought it best to report the issue. The behavior is completely repeatable.