STM32H7 ADC oversampling ratio define missing
With the newest CubeMx version 6.11.x, when selecting oversampling, a ratio is being set, and this ratio is a define, which are in "ADC_VER_V5_V90" that is not being set when a new project is created.
#if defined(ADC_VER_V5_V90)
#define ADC3_OVERSAMPLING_RATIO_2 (LL_ADC_OVS_RATIO_2)
#define ADC3_OVERSAMPLING_RATIO_4 (LL_ADC_OVS_RATIO_4)
#define ADC3_OVERSAMPLING_RATIO_8 (LL_ADC_OVS_RATIO_8)
#define ADC3_OVERSAMPLING_RATIO_16 (LL_ADC_OVS_RATIO_16)
#define ADC3_OVERSAMPLING_RATIO_32 (LL_ADC_OVS_RATIO_32)
#define ADC3_OVERSAMPLING_RATIO_64 (LL_ADC_OVS_RATIO_64)
#define ADC3_OVERSAMPLING_RATIO_128 (LL_ADC_OVS_RATIO_128)
#define ADC3_OVERSAMPLING_RATIO_256 (LL_ADC_OVS_RATIO_256)
#define ADC3_OVERSAMPLING_RATIO_512 (LL_ADC_OVS_RATIO_512)
#define ADC3_OVERSAMPLING_RATIO_1024 (LL_ADC_OVS_RATIO_1024)
#endif
This gives an error in the adc.c file as:
hadc1.Init.Oversampling.Ratio = ADC3_OVERSAMPLING_RATIO_4;
The "ADC3_OVERSAMPLING_RATIO_4" is missing/undeclared.