STM32H7 FDCAN clock issue
Hello all,
I have trouble running FDCAN on an STM32H742VG rev V when the cpu clock is above 300 MHz.
I have
D1CPRE = DIV1
HPRE = DIV2
D2PPRE1= DIV2
leading to the maximum allowed APB1 peripheral clock (= fdcan_pclk) for cpu clock >= 300 MHz (75 MHz for cpu clk = 300 MHz)
also I have HSE = 24 MHz used as FDCAN clk (= fdcan_ker_ck) and with FDCAN_CCU_CCFG.BCC = 1 and FDCAN_CCU_CCFG.CDIV=0 this is also fdcan_tq_clk and so fdcan_tq_clk is always smaller than fdcan_pclk.
But still this configuration only runs stable up to 300 MHz, at 330 MHz it fails after about a minute and with 360 MHz and above it does not work at all.
I have no trouble running UARTs, SPI, timers, ADC, DAC with cpu clk = 480 MHz, its only the FDCAN.
Did I miss something? Any known issues or workarounds?
Thanks for any hint
Martin