STM32H743bi - use FDCAN2 and USB ULPI simultaneously?
Hello,
I am using Cube32MX for STM32H743bi IO multiplexing. first i added USB HS phy ULPI interface then see FDCAN2 not allowed in the tool and error message says it is in conflict with USB ULPI. However i manually checked there were certain pins for CAN2 classic and even FD available.
I want to know whether it s some bug or there is some internal MCU sharing between these two that i am unaware of. Else several options are available for FDCAN2 after consuming USB ULPI.
thnx