[STM32H7B0RBT6][LTDC] Not possible to use RGB888 on CubeMx
Hello,
I am working on an HMI product with STM32H7B0RBTx LQFP64 and want to use the RGB888. As per Datasheet, it seems possible:

But when I start a project on CubeIDE, it only provides only RGB565/666.
My question is:
- Is this a limitation in the CubeMX and I can use RGB888 if I do it manually?
- If it's not the case, please to let me know and correct it on the datasheet.
Thanks,
Ayoub