STM32H7B3LIH6Q: Crystal Selection Impact on CubeMX Clock Configuration
Hello,
I am designing a custom board using the STM32H7B3LIH6Q, based on the STM32H7B3I-EVAL evaluation board. The crystal used on the evaluation board is 24 MHz, as seen from the schematic offered.
Now, I am building my own board and noticed that the part number used for the oscillator is not available. However, there the datasheet says this one can be a range (4 - 50 MHz). See datasheet snippet below.
My question is two fold:
- When they say "guaranteed by design" in the second note, does that mean that, if I use a crystal between 4-50 MHz, I can achieve the full 280 MHz clock frequency used by this MCU?
- Does choosing a crystal with a different frequency cause changes in the the CubeMX clock configuration?