Skip to main content
Associate
March 19, 2026
Question

stm32h7r7 linker misaligment?

  • March 19, 2026
  • 1 reply
  • 142 views

Hi there,

I've been using the STM32H7R7 device (BGA225), but I ran into an issue. I used the TochGFX (4.26) to generate the gfx_task, and after that, I configured the cubemx (6.17), but somehow the linker was not good. Even my code could not be built since the external PSRAM was not set up automatically. I fixed it, but I ran out of ideas. 
I would highly appreciate it if the demo were to be available to move forward. 

Thank you very much!
Geri

1 reply

Technical Moderator
March 23, 2026

Hello @geriTricky 

Could you please provide an .ioc file that demonstrates the problem.

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.