Skip to main content
Lukasz Nowak
Associate III
November 13, 2023
Solved

STM32U5 invalid SMPS warning during code generation

  • November 13, 2023
  • 1 reply
  • 2033 views

STM32CubeIDE 1.13.2 is showing a warning about SMPS for STM32U5 chips every time the code is generated (see attached).

This is done even for chips which do not have the SMPS pinout, e.g. STM32U595VJT (non Q), which is completely invalid.

But even when a chip does have SMPS, a designer may choose not to use it - why does this warning have to be shown every time the code is generated?

For reference CubeMX used in this version of IDE is:

Version: 6.9.2-RC4
Build: 20230910-1412 (UTC)

This topic has been closed for replies.
Best answer by STTwo-32

Hello again @Lukasz Nowak 

After check, I confirm that CubeMX should not allow to select the SMPS option in STM32U59xx device without SMPS.
Issue is reported internally to our team (Internal ticket number: 166485) and this will be fixed as soon as possible.

(PS: ID166485 is an internal tracking number and is not accessible or usable by customers)

PS: Issue solved on the last release of the STM32CubeMX

Thank you for reporting that.

Best Regards.

STTwo-32.

1 reply

STTwo-32
Technical Moderator
November 13, 2023

Hello @Lukasz Nowak and welcome back to the ST Community :smiling_face_with_smiling_eyes:.

Thank you for reporting this. I will check it internally and get back to you as soon as possible.

Best Regards.

STTwo-32

STTwo-32
STTwo-32Best answer
Technical Moderator
November 16, 2023

Hello again @Lukasz Nowak 

After check, I confirm that CubeMX should not allow to select the SMPS option in STM32U59xx device without SMPS.
Issue is reported internally to our team (Internal ticket number: 166485) and this will be fixed as soon as possible.

(PS: ID166485 is an internal tracking number and is not accessible or usable by customers)

PS: Issue solved on the last release of the STM32CubeMX

Thank you for reporting that.

Best Regards.

STTwo-32.