Target Software Startup Script Error
Hello All,
I am using STM32F777IITx MCU based custom board with STM32CubeMx v4.24.
I want to built a application where i want to Read/Write data from/to flash.
I am have written a small application where i write 10 bytes of data to flash and also read those 10 bytes from flash
My code Complies properly with no errors, However, when i tried to run the code in Debug mode i am getting the error mentioned below.

Whereas i have not changed anything in the Startup script, also i have attached the startup script below
# Set flash parallelism mode to 32, 16, or 8 bit when using STM32 F2/F4 microcontrollers
# 2=32 bit, 1=16 bit and 0=8 bit parallelism mode
monitor flash set_parallelism_mode 2
# Load the program executable
load
# Enable Debug connection in low power modes (DBGMCU->CR)
set *0xE0042004 = (*0xE0042004) | 0x7
# Set a breakpoint at main().
tbreak main
# Run to the breakpoint.
continueSo please help me to get rid of this issue at the earliest and if i am making any mistake while debugging please help me with it ,
Also if there are changes to be made in startup script please help me with correct startup script
Thanks and Regards
Utkarsh