The mouse wheel doesn't scroll the STM32CubeMX Categories window in most places
In STM32CubeMX v6.17.0, in the left side of the Pinout & Configuration panel, if the mouse cursor is within a table that lists peripherals, the scroll wheel doesn't do anything. I expect it to scroll the window. You need to move it outside of the table but still within the bounds of the "Categories" tab in order to scroll up and down. This is super annoying because it means you have to have the cursor on the far left or far right of this window otherwise a table will appear when scrolling and the mouse wheel will stop working.
In the screenshot, having the cursor anywhere in the red box will stop it from scrolling. I expect it to scroll the green scrollbar.