Skip to main content
RMeda.1
Visitor II
March 27, 2023
Question

The STM32U575 MCU can not use a 4 Bit SD card in 4 bit mode. Using the driver and FAT32 from qubeMX result in an error. The error is that the bits are shifted by 4 bits. What do i do wrong or is this a known issue. If it is an issue, is there a quick

  • March 27, 2023
  • 1 reply
  • 1148 views

..

This topic has been closed for replies.

1 reply

jaw
Associate
March 12, 2024

did you even get anywhere on this?

 

I'm seeing the same issue on the 'U5A5. 

works perfectly in 1-bit mode. but 4-bit mode fails (even with the clock at 400kHz)

nothing mentioned in the errata.

AScha.3
Super User
March 12, 2024
"If you feel a post has answered your question, please click ""Accept as Solution""."