Question
This is an inquiry regarding STM32G031 PF2-NRST, PA14-BOOT0 Pin settings.
I am using the STM32G031 MCU, and if you look at the picture below in the STM32 CubeMX,
there are no NRST and BOOT0 settings at the PF2-NRST and PA14-Boot0 Pin


I am curious as to whether it is set as default even if I do not configure it, or if there is a way to set it separately. help!!