Trigger SPI DMA transfer from Timer directly
Hey there,
at the moment I am stuck with the following problem: I need to trigger a SPI DMA Transfer precisely at each Timer overflow. NVIC Timer interrupts are not an option, because the jitter is way too high when I have to jump into code each time (I managed to trigger SPI-DMA transfer using the Timers NVIC global interrupt, but as I said, jitter is way too high). So now I am looking for a solution that involves the Cube MX, I want to configure the Timer in a way so that it directly triggers the DMA of the SPI? Or is there anything I can once declare in code that will do the job for me? In the end the solution should work without the CPU at all. I am using a NUCLEO-F446RE Board here, running at 180MHz. If someone has a quick solution (In Cube MX or Code, doesn’t matter as long as it works) I would be very thankful!
Greetings Julius