Unable to save modified .ld file when CubeMX generates the CMake project
I used CubeMX to generate CMake project for STM32H750XBH6.

Then I have to modify STM32H750XBHx_FLASH.ld because DMA1 can't access the DTCMRAM.
/* Specify the memory areas */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K
} /* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >DTCMRAMBut everytime I use CubeMX regenerate the project, STM32H750XBHx_FLASH.ld will be recovered. My changes didn't save.
How can I save this modified STM32H750XBHx_FLASH.ld when CubeMX regenerates project?