Skip to main content
Associate II
August 8, 2024
Solved

USART3 not available to use in CubeMX

  • August 8, 2024
  • 2 replies
  • 2349 views

I am trying to generate code using CubeMX (version 6.11.1), using the NUCLEO-H563ZI board to start the project. But, I am getting the following pop-up when trying to use the USART3 peripheral which seems to be unavailable:

AShetty_0-1723109965194.png

Because of this, I had to downgrade the version of CubeMX to 6.10.0 to use USART3. However, I observed that even after saving the ioc file, later when we opened the file again CubeMX had overwritten the pins to the default state.

AShetty_1-1723110323714.png

Why is this happening and is there any workaround for it?

Best answer by STTwo-32

Hello @AShetty 

When you start your project, you have to disable the generation of the Human Machine Interface using the Button "Unselect All" then ok to open you .ioc file.

STTwo32_0-1723118790157.png

Best Regards.

STTwo-32

2 replies

Andrew Neil
Super User
August 8, 2024

Did you look at the "Details & documentation":

AndrewNeil_0-1723110600245.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AShettyAuthor
Associate II
August 8, 2024

That is just the data sheet and the reference manual.

AScha.3
Super User
August 8, 2024

This is the VCP , on USART3 on this board connected, so its already used - so it shows this to you.

If you wnat to use it, you have to cut the connections on the board and make your hardware then to the rx/tx PD8/9 .

Why not using it as intended for VCP (or debug printf(...) ) ?

see circuit of this board:

AScha3_0-1723115028824.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
AShettyAuthor
Associate II
August 8, 2024

The application I am using is not using these pins for debugging purposes but rather to send data from the board to the PC. 

I am able to generate code by unlocking the pins and enabling USART3 in CubeMX 6.10.0. But CubeMX seems to overwrite it again to VCP when I open the file again.

One workaround I found was to use STM32H563ZIT6 MCU instead of the NUCLEO board before starting the project in CubeMX. Is there no resolution to this in the NUCLEO-H563ZI board project?

STTwo-32
STTwo-32Best answer
Technical Moderator
August 8, 2024

Hello @AShetty 

When you start your project, you have to disable the generation of the Human Machine Interface using the Button "Unselect All" then ok to open you .ioc file.

STTwo32_0-1723118790157.png

Best Regards.

STTwo-32