USB_VBUS available on STM32G0B1CET6N?
I want to use the STM32G0B1CET6N and communicate to this device using USB Full Speed (FS).
I chose this model, because it has the internal "HSI48 RC" Oscillator, which can direclty supply a 48 MHz clock to the USB device.
Thats the configuration:

The STM32 will act as a "Communication Device Class (Virtual Port Com)"

I want to supply my whole PCB using the Power from the USB Port from my Laptop (5V/500mA). So I read about the "USB_VBUS"-Feature, which I think would make sense for my application.
I found this in the Datasheet:

I was not able to find the "USB_VBUS" activate Box in the CubeMX configurator!
So thats why I think, that this model maybe does not support this option....however the Datasheet says otherwise.
I am confused! Maybe it is always active, as soon as you enable USB connectivity? Please help me.