Skip to main content
Associate II
February 6, 2025
Solved

VREFBUF can't set to internal with new MX Version (+VDDA isolation is forced)

  • February 6, 2025
  • 1 reply
  • 1474 views

Hello everyone,

I have a project with an STM32U575VGT6. This was created with STM32CubeMX version 6.8.1. Now the project should be made compatible with the latest IDE version (V1.17.0) as part of a larger conversion action and for this purpose a migrate of the ioc was carried out (STM32CubeMX version 6.13.0).
In the original project, VREFBUF was set to ‘Internal voltage reference’ mode with ‘SCALE0’.
After the upgrade, this selection is no longer available and VREFBUF is set to ‘Disabled’ by default.
I have also noticed that since the upgrade there is the option ‘isolation Vdda’ under ‘PWR’, which cannot be deactivated.

Ultimately, this means that 0V is applied to the Vref pin and the ADC and DAC do not function correctly.
What has been changed here and what do I have to set so that my application works again?

Many thanks for your help
Robert

old Version:

rohe_0-1738836515224.png

new Version:

rohe_1-1738836542946.png

rohe_2-1738836571334.png

 

Best answer by Mahmoud Ben Romdhane

Hello @rohe ,

Internal voltage reference is missing from the VREFBUF mode. This issue was reported (under this internal ticket 199643). I suggest that you take a look at this Thread.

Thanks.

Mahmoud

 

1 reply

roheAuthor
Associate II
February 6, 2025

The reference manual states that VREF+ is not available for some packages and is double-bonded with VDDA.

rohe_1-1738837699769.png

However, the package I am using should not be affected by this (after all, it already worked with the old software version).

rohe_0-1738837419786.png

Could it be that there is a bug in the CubeMX software that it assumes that VREF and VDD are double-bonded in my package as well?

 

Technical Moderator
February 6, 2025

Hello @rohe ,

First let me thank you for your feedback and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Technical Moderator
February 6, 2025

Hello @rohe ,

Internal voltage reference is missing from the VREFBUF mode. This issue was reported (under this internal ticket 199643). I suggest that you take a look at this Thread.

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.