Wakeup pins for STM32F030xC are missing in CubeMx
Hi everyone.
I am selecting in CubeMX STM32F030xC MCU.
I see on the screen case where STM32F030CCTx LQFP48 is written.
Then I open Datasheet. There is Table 1. Device summary.
STM32F030xC corresponds to STM32F030CC and STM32F030RC.
Ok. Then I look at pinout.
There is PA2 (pin 12). It is WKUP4 (5).
At (5) there is: For STM32F030xC devices only
But in CubeMX there is no WAKEUP for PA2 (pin 12) when I open pin properties.
What I am missing?
I have another question related to WAKEUP pin configuration in CubeMX.
Wakeup triggers on rising edge so normally it must be pulled down.
But when I set available WAKEUP pins I can't select pull down explicitly in CubeMX menu.
Maybe CubeMX does that implicitly?
Thanks