How can I use multiple decision tree with the MLC of a LSM6DSOX Good afternoon everyone,I am currently working on a predictive maintenance projet using vibration classification with the MLC of a LSM6DSOX.I would like to try using several decision tree at the same time (with a maximum of 8 according to the datasheet), 3 for example.I have some trouble to build my .ucf file.I tried to do exactly the same than with a single decision tree, but it does not work.Actually I can build it the .ucf file, but I am getting "0x00" (default value) output in every channels of my MLC, whereas it should not be possible with the configuration I made.So I think I made a mistake during the configuration step on Unico, but I cannot see it.Maybe there are requirements I did not follow, or I may have to change my MLC configuration ...Is there any tutorial that explain how to configure the MLC with several decision tree ? Or can anyone explain me my possible mistake ? Thank you,Have a nice day,Julien.