How to send command to the NOR flash using SPI? I'm using STM32L4A6VGx , MT25QL256 NOR Flash connected with SPI. I'm trying to read the ID but didn't get any response except 0. Here is the code I wrote: // Select Pin HAL_GPIO_WritePin(Select_GPIO_Port, Select_Pin, GPIO_PIN_SET); HAL_Delay(10); HAL_GPIO_WritePin(Select_GPIO_Port, Select_Pin, GPIO_PIN_RESET); Dev_ID[0] = 0x09E; HAL_SPI_Transmit(&hspi2, Dev_ID, 1,10); HAL_SPI_Receive(&hspi2, &Dev_ID[1], 1,10); HAL_GPIO_WritePin(Select_GPIO_Port, Select_Pin, GPIO_PIN_SET);//SPI Configurationstatic void MX_SPI2_Init(void){ /* USER CODE BEGIN SPI2_Init 0 */ /* USER CODE END SPI2_Init 0 */ /* USER CODE BEGIN SPI2_Init 1 */ /* USER CODE END SPI2_Init 1 */ /* SPI2 parameter configuration*/ hspi2.Instance = SPI2; hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CL