Skip to main content
istepne
Associate III
July 17, 2024
Solved

ADC1_IN16 uasge

  • July 17, 2024
  • 2 replies
  • 1032 views

Hi,

I am using the latest version v1.16.0 STM32CubeIDE with stm32g071cb.
It is not possible to use ADC1_IN16 (PB12). I have created also a new project  to test this condition.
Changing the sequencer disables IN16 or makes error condition.
I need PA2 -PA3 and PB12 pins (IN2-3-16 channels to ADC sampling)
Below attached screen view and the ioc file generated via STM32CubeIDE

istepne_1-1721201408556.png

Regards

Murat

 

 

 

    Best answer by STTwo-32

    Hello @istepne 

    This issue has been reported in this post and it will be solved on the coming Cube Tools Releases.

    Update: this issue has been solved on the STM32CubeMX V6.13.0.

    Best Regards.

    STTwo-32

    2 replies

    STTwo-32
    STTwo-32Best answer
    Technical Moderator
    July 17, 2024

    Hello @istepne 

    This issue has been reported in this post and it will be solved on the coming Cube Tools Releases.

    Update: this issue has been solved on the STM32CubeMX V6.13.0.

    Best Regards.

    STTwo-32

    carlesls2
    Associate III
    March 20, 2025

    How do you chhnage the sequencer?

    Thanks 

    istepne
    istepneAuthor
    Associate III
    March 21, 2025

    I am using the latest update Version: 1.18.0

    Stil it can not be changed as "fully configurable".

    Also I am using 9channels enabled DMA transfer and the transferred data order is not same as cahnnel selection.

    To get ADC sample on channel IN16, I have to choose "not fully compatible". And as a transfer result of the converted ADC value placed in order with In7-Temp-Vref-In11-Vbat-IN16 (not shown below)

    So, still some problems

    istepne_0-1742545729184.png

     

     

    carlesls2
    Associate III
    March 21, 2025

    Thanks. It worked