As a result of updating CubeIDE to V1.16.0, program transfer to MCU inevitably fails.
After updating CubeIDE to V1.16.0, I get an error like "Data mismatch found at address 0x08001000 (byte = 0xFF instead of 0x0E)" and cannot complete the debugger. This error text was obtained from the Internet with similar symptoms, except for the address number, etc.
I have tried all the solutions available on the Internet, but none of them worked. I also installed and tried CubeIDE released in the past, but it did not work.
Before the update, I was able to complete the debugger reliably.
Development Environment
CubeIDE V1.15.1 or V1.16.0
ST Link V3MINIE