Compile old project with newest CubeIDE: flash size increased & application not working
Hello,
I need to modify an old application which has initially been created with Atollic TrueStudio and was then adapted to an early version of CubeIDE. It's a project from a colleague who has retired.
From what I can see so far is that the projects .ioc file was made with a version 6.5 or older (CubeIDE throws an error about it if I try to open it). However, thanks to the project PDF report I was able to recreate the .ioc file with the original device settings. I copied the application sources without modifications and created the project.
Unfortunately, the application does not work, so I'm trying to figure out what's going wrong. From what I can see so far is that the interrupts seem to be correctly enabled and the handlers are called (currently I could verify this only for SysTick, for the other interrupts I need to create a dedicated test setup).
But the original generated code makes calls to the corresponding peripheral handlers from the interrupt handlers which are either missing in the new generated code (e.g. SysTick, there's no automatically available callback) or it might be that the empty, weak default functions are called instead of the 'strong' handlers - as written above, I can verify this only after the test setup is up and running.
Also, it looks like the way to make the corresponding setting in the CubeMX view has changed (enabling interrupts and enabling the generation of interrupt related code seems to be at other places now).
So, in case of that I've overlooked something, any hints about where I should look at in the .ioc configuration is appreciated.
A second question is about the consumed flash size of the binary. The original one took ~8kByte, the new one takes ~12kByte. Since I didn't modify the application source files and the project doesn't use floats or printf() etc I wonder if this should be expected or if there's a (new) setting within the build options which I'm not aware of. Things like compiler/linker optimization settings, etc are identical between the old and the new project files as far as I can see.
Regards