"Could not determine GDB version" running on Linux 24.04 LTS Noble
- November 19, 2025
- 3 replies
- 514 views
Hi all I am a newbie to Linux and I badly want to excel in the system and currently i've stumbled upon an issue of not being able to run and debug my code to STM32-NUCLEO-F4460RE board through CUBE IDE. On running the program to my bord its i showing an error window and giving error message "Could not determine GDB version using command: arm-none-eabi-gdb --version". I asked Gemini and Chatgpt for help and got replies that made me symlink my libncurses.so.6.4 to .so.5 and similarly with libtinfo, then I installed gdb-multiarch as I was not able to download arm-none-eabi-gdb even with .gcc. Even I changed the prefernce to gdb-multiarch and its still the same. To add my Linux version is 24.04 LTS Noble. Kindly someone help me out of this mess.