CubeIDE 2.1.1 wrong linker script memory definitions for STM32C562RE
Hello,
I just downloaded STMCubeIDE 2.1.1 to generate a simple project for a Nucleo-C562RE board.
I am not using CubeMX2 (for various reason, that is not the point).
The default empty project generated for STM32C562RE by the IDE has only 1 SRAM element with a size of 64K, instead of 2 SRAM elements of 64K each.
FLASH size is correct though.
Out of curiosity, if ST were to push a fix for this kind of bug, would it be a new IDE release ? or could it be a STM32C5 pack update only ?