Skip to main content
Armadillo
Visitor II
April 28, 2025
Solved

CubeIDE CubeMX UI unusual

  • April 28, 2025
  • 1 reply
  • 360 views

Hello,

When I launch CubeMX from the CubeIDE via New Project the UI of CubeMX appears unusual. The sidebars are "Windows XP style" and there are other graphical anomalies. When I launch CubeMX from VScode the UI appears normal. The two screenshots I posted show the differences. I am wondering if maybe there is some setting in CubeIDE that may have caused this.

Thanks

 

 

Best answer by STTwo-32

Hello @Armadillo and welcome to the ST Community.

this is a known limitation mentioned on the STM32CubeIDE V1.18.x errata wikiAfter updating the STM32CubeIDE from some versions to the patch 1.18.1 using the update site updater, the GUI of the integrated STM32CubeFinder and STM32CubeMX are the images of the old UI tools.

Workaround: reinstall STM32CubeIDE from the installer on st.com.


Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
Technical Moderator
April 28, 2025

Hello @Armadillo and welcome to the ST Community.

this is a known limitation mentioned on the STM32CubeIDE V1.18.x errata wikiAfter updating the STM32CubeIDE from some versions to the patch 1.18.1 using the update site updater, the GUI of the integrated STM32CubeFinder and STM32CubeMX are the images of the old UI tools.

Workaround: reinstall STM32CubeIDE from the installer on st.com.


Best Regards.

STTwo-32