CubeIDE does not have "STM32 project" option in "Create New STM32 Project" subsection
Hi, I have a problem with my CubeIDE installation that is that I cannot create a stm32 project(the option that integrates with CubeMX) I can only create the following

I've installed it from the shell script from the generic Linux download, I'm using arch Linux(btw).
I've reinstalled it at least 3 times now, also went to Help -> Install New Software, used this site:

And installed everything down the STM32CubeIDE section.