Skip to main content
TJM
Senior II
February 26, 2026
Question

CubeIDE v1.19 and v2.0.0 - very high CPU usage on Linux

  • February 26, 2026
  • 2 replies
  • 221 views

Good morning.

Using CubeIDE both v1.19 and v2.0.0 with Debian Linux v11.11.

I'm seeing very high processor usage, 300% and higher, all of it java based even when there is no activity in the IDE.  Is there an explanation available for this usage, or is there a way to bring the usage back down out of the stratosphere, or is there just a leak that's causing this?  It doesn't really appear to be affecting anything bigtime so this is just an information inquiry.  System monitor screenshot attached.

Just for information, I was using IDE v2.0 for a few days then found it upgraded to v2.1.  v2.1 uses a later version of libc and doesn't run on my Debian 11.11 system.

 

SysMonitor.png

 

Thanks,

TJM

 

2 replies

AScha.3
Super User
February 26, 2026

Hi,

i am on LinuxMX , have about 0.5% cpu load with browser + stm32-IDE (V 1.18.1 ) running.

+ on compile/link it can reach 100% for some seconds, all 8 cores busy - but thats expected, right ?

 

>I'm seeing very high processor usage, 300% and higher

How you can get > 100% ?   warp drive ?  (btw 100% = full max load , so...?)

"If you feel a post has answered your question, please click ""Accept as Solution""."
TJM
TJMAuthor
Senior II
February 26, 2026

Over 100%, yes, it's adding up the percentages across all the cores.  Something is going on in the background that keeps java busy.  Just trying to figure out what it is.

 

 

AScha.3
Super User
February 26, 2026

Hmm...ok,

so switch off all "online services" and auto-update etc. , as this always searching for ...who knows.

 

Now i cannot post pics.. this forum is worse than any hobby beginners forum...not working to post pics now.

 

come on...who is driving this ? some unknown guys , first time building a "forum" ???

sorry...but look at some forum, that is really built from old guys, doing their hobby :

https://www.radio-bastler.de/forum/

THIS is working, adapt dark style...etc. as it should be. Maybe STM should ask them for help.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TJM
TJMAuthor
Senior II
March 4, 2026

Thanks for the suggestions, I'll try those.  I posted a pic of the processor usage but it didn't post.

 

Tony