CubeIDE version 2.0 lacking adequate selection assistance
Previous versions of cube had very nice board seelction tools.
At the top of the screen was aa complete board descrription that enabled the easy selection of board features when starting a new project and wanting to see what peripherals were available on the board and chip
The current version 2.0 has very, very sparse information, inadequate to find out which boards havee what preipherals. The facility is easyt to provide since it simply references the sales literature available on the ST site.
This information is not even available by double clicking on the products offered in the IDE.
Furthermore, the online product selector is almost useless, there are 3 columns with identical headings under ADC converters. I presume these refer to differrent ADC capabilities, but am left in the dark as to their meaning.
I understand that this might be a seldom used function, occurring once or twice in a product lifecycle, yet it is an invaluable tool.
The filters are also very cumbersome when compared to the left hand tab selector of previous cube versions.
Altogether a regressive step and a very cumbersome experience.
I guesss that sadly, I will need to install an older version of cube alongside the new one.
Am I the only one with this observation?