.d:1: *** multiple target patterns. Stop.
From cube 1.3.0 I always get this error and the cause seems to be the path generation in .d files. In cube 1.12.1 the path is relative but from cube 1.3.0 it is absolute and generates something like \\?\C:\.... So the only solution for me is to stay with cube 1.12.0. The build however seems ok an the bin file is generated. Did anyone had a similar issue? The issue is present only on windows and it seems ok on linux.
arm-none-eabi-size STM32F769I_TEST.elf
arm-none-eabi-objdump -h -S STM32F769I_TEST.elf > "STM32F769I_TEST.list"
arm-none-eabi-objcopy -O ihex STM32F769I_TEST.elf "STM32F769I_TEST.hex"
arm-none-eabi-objcopy -O binary STM32F769I_TEST.elf "STM32F769I_TEST.bin"
text data bss dec hex filename
1227608 43680 452264 1723552 1a4ca0 STM32F769I_TEST.elf
Finished building: default.size.stdout
Finished building: STM32F769I_TEST.hex
Finished building: STM32F769I_TEST.bin
Finished building: STM32F769I_TEST.list
test/web/unicabminnow.d:1: *** multiple target patterns. Stop.
make: *** [makefile:152: all] Error 2
"make -j8 all" terminated with exit code 2. Build might be incomplete.
12:23:07 Build Failed. 3 errors, 408 warnings. (took 1m:27s.726ms)