Skip to main content
Associate II
September 24, 2025
Question

Did not get SWV prints in STM32CubeIDE

  • September 24, 2025
  • 10 replies
  • 1226 views

Hii Everyone, I am trying to debug with SWO and SWV in STM32CubeIDE with NUCLEO-H753ZI. But, I am not getting any prints on SWV ITM Data console. As you can see all settings in the below attachments. My CPU system clock is running at 400Mhz. Anyone suggest me to get prints in SWV/ITM Data console.

SDTAN0907_0-1758694249404.pngSDTAN0907_1-1758694368626.pngSDTAN0907_2-1758694433406.png

 

SDTAN0907_3-1758694547143.png

 

10 replies

KDJEM.1
Technical Moderator
September 24, 2025

Hello @SDTAN0907 and welcome to the community;

 

Are you able to see the message in another terminal?

Which STM32CubeIDE version are you using?

Could you please share your project?

I recommend you to look at AN4948 precisely section "7.3 Printf via SWO/SWV" may help you.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SDTAN0907Author
Associate II
September 26, 2025

hii @KDJEM.1 ,

 

Thank you for your response.

I have followed same procedure as mentioned in this document AN4948. But I didn't get any prints.

Yes, the message is showing up correctly in QCOM(UART Communication).

STM32CubeIDE version : 1.19.0.

I have attached project file in the attachment tool bar. Please give me solution to get prints in SWV ITM data console.

 

Thanks & Regards,

Divya.

 

 

 

Pavel A.
Super User
September 26, 2025

To start the ITM trace you need to wait until the debugger stops at the first breakpoint, usually at main.

Then click the icon on the ITM console toolbar, as shown: It should change color to RED. Then resume execution.

PavelA_0-1758902792040.png

Also, try to limit the SWO clock: up to 4 or 8 MHz, not 12.

 

SDTAN0907Author
Associate II
September 26, 2025

Hii @Pavel A. 

Thank you your reply, I did same thing as you said. But I didn't get any prints.

Pavel A.
Super User
September 28, 2025

The ITM trace is sometimes very hard to get working, of no clear reason. Try other software, for example, CubeProgrammer to view the prints.

 

SDTAN0907Author
Associate II
September 30, 2025

I have done with CubeProgrammer. In that application also, I didn't get any prints

 

Pavel A.
Super User
October 1, 2025
SDTAN0907Author
Associate II
October 3, 2025

I did the same way as mentioned in the above thread. But I didn't get any prints.

Pavel A.
Super User
October 3, 2025

Then, maybe, software regression? I don't use the latest cubeide yet. Try to view ITM in cube programmer.

PHolt.1
Senior
October 3, 2025

There is a weird issue with that red button. Cube IDE has the wrong mouseover text on it. See

https://www.eevblog.com/forum/microcontrollers/stlink-debugger-configures-some-32f4-target-registers-e-g-swo-trace-macrocell/msg6054427/#msg6054427

But it works better if you Detach the SWV ITM tab and have it standalone. See above thread.

Also see e.g. here

https://community.st.com/t5/stm32-mcus-boards-and-hardware/32f417-how-to-use-swv-itm-swo-debug-output-without-cube-ide-or/td-p/843611/page/3

SWV ITM can be very hard to get working. It works better in the OpenOCD (not the default GDB Server) debugger mode (still with STLINK) as shown above. GDB Server works fine for normal flashing of the code, and breakpoints and such.

If you check PC Sampling (needed for statistical profiling) then the whole thing gets much less reliable. The debugger needs to be power cycled (USB unplugged and replugged) after each collection session, plus Cube exit and restart.

There is a config in Cube for the buffer size. I use 20MB.

SDTAN0907Author
Associate II
October 3, 2025

Thank you for your reply,

I tried using OpenOCD for SWV debugging, but I still don't see any output in the SWV Viewer. I've attached my project files, OpenOCD config and GDB debugger settings, and SWV configuration. Could you please review them and let me know if there's any misconfiguration or missing setup that might be preventing the SWV prints from appearing?"

SDTAN0907_0-1759492960039.png

SDTAN0907_1-1759492989251.png

SDTAN0907_2-1759493078505.png

 

 

PHolt.1
Senior
October 3, 2025

I use SWD frequency 8000kHz (not Auto). AFAICT the auto mode tries different speeds and it can discover a "working" speed which is marginal. I never go above 8000kHz, not even with the STLINK V3 MINIE which should be the fastest (but has other problems).

Also uncheck Enable Prescaler.

Last post here

https://community.st.com/t5/stm32-mcus-boards-and-hardware/32f417-how-to-use-swv-itm-swo-debug-output-without-cube-ide-or/td-p/843611/page/3

And ALWAYS EXIT AND RESTART CUBE IDE after any debugger related config change, plus unplug and replug the debugger USB cable. The parameters in the 1st form do not get picked up in the 2nd form except when Cube it restarted (you can prove this anytime).

I am right now testing the STLINK V3 MINIE and find that the SWV ITM debug works only if I fix the SWO clock to 1000kHz, not Auto. The debugger clock is still 8MHz. This is weird because this one has no isolation so should be super fast. And of course statistical profiling does not work at all. This is with a 12cm cable, too.

SDTAN0907Author
Associate II
October 3, 2025

I tried with 8000KHz and different frequencies, unchecked Enable Prescaler. But still I don't get prints. I have observed one point, kept a break point at this line

bItmAvailable = 1 ;

Execution goes to that line, it means port 0 is not ready to accept new data. I don't understand why it is happening. You have any idea, Please guide me.

SDTAN0907_0-1759500703402.png

 

PHolt.1
Senior
October 3, 2025

Are you calling the right function? Try this and output just one char or a string.

/*
 * Copied here from core_cm4.h.
 \brief ITM Send Character
 \details Transmits a character via the ITM channel 0, and
 \li Just returns when no debugger is connected that has booked the output.
 \li Is blocking when a debugger is connected, but the previous character sent has not been transmitted.
 \param [in] ch Character to transmit.
 */

static void ITM_SendChar_2 (uint32_t ch)
{
 if (((ITM->TCR & ITM_TCR_ITMENA_Msk) != 0UL) && /* ITM enabled */
 ((ITM->TER & 1UL ) != 0UL) ) /* ITM Port #0 enabled */
 {
 while (ITM->PORT[0U].u32 == 0UL)
 {
 __NOP();
 }
 ITM->PORT[0U].u8 = (uint8_t)ch;
 }
 return;
}


// This sends debug output to the SWV ITM / SWD debug interface
// was: __io_putchar(int ch) - this was for the old ST-supplied printf
int _putchar (int ch)
{
 ITM_SendChar_2(ch);
 return ch;
}

 The putchar is to make printf() output to SWV ITM but it depends on your printf() code.

You don't need the SWO config. The debugger does it for you: Your swoinit() is superfluous.

https://community.st.com/t5/stm32-mcus-boards-and-hardware/32f417-how-to-use-swv-itm-swo-debug-output-without-cube-ide-or/td-p/843611/page/3

https://www.eevblog.com/forum/microcontrollers/stlink-debugger-configures-some-32f4-target-registers-e-g-swo-trace-macrocell/msg6054105/#msg6054105

 

SDTAN0907Author
Associate II
October 3, 2025

I am calling that function. Execution goes to this line also 

ITM->PORT[0U].u8 = (uint8_t)ch;

But, I don't get any prints. I have attached image and updated project file.

SDTAN0907_0-1759507167121.png

STM32CubeIDE Version : 1.19.0

STlink upgarde version info

SDTAN0907_1-1759507427496.png

STM32CubeMX Version : 6.15.0

 

PHolt.1
Senior
October 3, 2025

In that case, check with a scope for data coming out of the SWO pin on the CPU.

 

PHolt.1
Senior
October 6, 2025

In that case either the debugger is not configuring the trace macrocell correctly or, more likely, you have put in some code which wipes out that initialisation.

You should see stuff on the scope at the correct timing e.g. with a 168MHz CPU clock, SWO limited to 1MHz, you should see 1us-spaced transitions on the scope.

SDTAN0907Author
Associate II
October 6, 2025

I have removed that code what I have previously included and verified the output at that pin with CPU clock 168MHz, SWO limited to 1MHz. But still I didn't see any data on that pin.

PHolt.1
Senior
October 6, 2025

All I can suggest is you build a second target.

One should always build TWO boards, because a single target can be dud for any of many reasons.