Skip to main content
Jack3
Senior
October 25, 2024
Question

Dual-Core project - how to add driver in project tree under CM7?

  • October 25, 2024
  • 1 reply
  • 648 views

Hello,

I'm starting a dual-core project .
But how do I add a driver in project tree under CM7 in the directory MyProject\CM7\Drivers\STM32H7xx_HAL_Driver?

I have copied (manually) stm32h7xx_hal_pcd and stm32h7xx_ll_usb drivers into this directory MyProject\Drivers\STM32H7xx_HAL_Driver (Inc and Src).

So, on disk and in the Project Explorer, I can see those in MyProject\Drivers\STM32H7xx_HAL_Driver.

However, in de Project Explorer, in CM7, I find files in MyProject\CM7\Drivers\STM32H7xx_HAL_Driver, except the ones I added in the previous directory. On disk I see no files in MyProject\CM7\Drivers\STM32H7xx_HAL_Driver.

Are those somehow linked in the project?

How can I do that? I dragged the files from the first directory into the second and selected 'Link to files'.
But that doesn't work, the compiler complaines it misses the files.
Hard copying them on the disk to the second directory works, but it seem ugly.

Does anybody know the correct way to do it.

 

Is this the correct way?

1 reply

Jack3
Jack3Author
Senior
January 15, 2025

I know how to do it correctly, but by editing the project files. It seems the only way, if you don't want to used STM32CubeMX, after starting the project. STM32CubeMX has its bugs and will restore those you fixed, if you let it replace code parts.