Solved
Error in final launch sequence - No device on target
- February 5, 2025
- 7 replies
- 4742 views
I have a NUCLEO-G491RE board connected to a PC running STM32CubeIDE v1.17.0. On first connection I was prompted to update the firmware on the board, which I did. On successful completion of the update I disconnected and reconnected the board, but the download failed with the attached message.
I have tried several USB cables and also with and without an intermediate USB hub to eliminate these possibilities.
What is the solution please?