Errors with my project
- December 3, 2024
- 1 reply
- 708 views
From a previous discussion and new thread created for new question:
Hello, thank you for your early reply.
I'm missing the STM32F429I_DISCO_REV_E01.ioc file.
I try to add same simple Code to the Mail file in User section...
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
// HAL_GPIO_TogglePin(GPIOx, GPIO_Pin)
HAL_GPIO_TogglePin(GPIOG, 13); // LED I want to look for LD3 ore LD4
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
I got this error message....
If I debug the Programm I got the Errors in the grafik.png, and the programm look like Stop.
I can't find the LD3 and the LD4 in the AutoCompled ....
so I think they are not configured. May be this a problem of mine, I don't anderstand
And short before I write my code, i see this comment
/* We should never get here as control is now taken by the scheduler */
Now I add the by "STM32 from a existing STM32CubeMX.ioc file.
after it. This will work with no error. Than i config GPIOG_pin13 and Build again, lots off errors occure.
How i can change the STMCubeMX file ?
Sorry, for the time you spend. Hope we mamage the Problem.
Thank you in advance , Peter