Skip to main content
Associate
November 26, 2023
Solved

Failed to Generate Command line

  • November 26, 2023
  • 3 replies
  • 5292 views

Hi there,

I'm new to this community. I'm having an issue right now. Everything was working fine, until I made the mistake of going to Project -> Properties -> settings -> C/C++ Build -> Settings. Silly me hit "restore defaults"

Ever since that moment, when I hit the Hammer Icon to build, I get errors that say "Failed to Generate Command line. Reason: Unknown Target".

I"m assuming somehow I deleted the linker settings somehow? 


I also get these issues. 

Teyros_0-1701004655141.png

"Drivers/STM32G4xx_HAL_Driver/Src/subdir.mk:73: *** unable to generate command line. Stop."

Would really appreciate some help on how to fix this, thanks so much.

Regards,
Teyros

    Best answer by Teyros

    OK So in the end, it appears I couldn't give the STM32cubeIDE a new target, it was greyed out. 
    So I selected the option to create a new project with an existing ioc file. Then dragged and dropped all the src and inc files. Seems to work now when I select build.

    Teyros_0-1701039625347.png

     

    3 replies

    TeyrosAuthor
    Associate
    November 26, 2023

    Could really use some help guys/gals.

    I created a new file, and it appears that the HAL drivers under Debug are deleting themselves. 

    Teyros_0-1701038244198.png

     Also noticed I cant get the MCU and Board options to be available how do I get that to select the board?



    Whenever I copy and paste the working new files Debug HAL drivers in, when I click build, then they get removed and that same error happens again

    TeyrosAuthorBest answer
    Associate
    November 26, 2023

    OK So in the end, it appears I couldn't give the STM32cubeIDE a new target, it was greyed out. 
    So I selected the option to create a new project with an existing ioc file. Then dragged and dropped all the src and inc files. Seems to work now when I select build.

    Teyros_0-1701039625347.png

     

    Technical Moderator
    November 27, 2023

    Hello @Teyros ,

    First let me thank you for posting and welcome to the ST Community.

    You are not compiling certain source files that are under Drivers/STM32G4xx_HAL_Driver/Src. Maybe you have deleted a folder from this list.

    Thanks.

    Mahmoud.

     

     

     

     

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    TeyrosAuthor
    Associate
    November 30, 2023

    Hi Mahmoud,

    Thanks for the welcome. Yes in the end when I restored default, it removed the target from the settings. I was unable to modify and reset the target, but creating a new file and copying my .c and .h files seemed to be a good temporary solution. 

    Hope you are well,

    Regards,

    Teyros

    Visitor II
    January 27, 2025

    Hi, Maybe you need to install last version of STM32CubeIDE.