Skip to main content
Associate
October 9, 2024
Solved

FreeRtos error in STM32H7

  • October 9, 2024
  • 2 replies
  • 2366 views

 

Hello,

I am working with stm32H755 and FreeRTOS. After setting up debugger, I start debugging the program. the code is built fine, then get this error msg(attached picture) only if i enable FreeRTOS from the setup window(attached picture) . But i need to use freeRTOS. How can i solved this issue? 

Any support is welcome.

Thanks

1. in the freertos.c file, The code is

void MX_FREERTOS_Init(void) {

 osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 8192);
 defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);

}

2. debug msg

STMicroelectronics ST-LINK GDB server. Version 7.3.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Exit.

```

Settings in STM32CubeIDE1.12.0Settings in STM32CubeIDE1.12.0error messageerror message 

Best answer by mƎALLEm

OK since it's a custom board you need to check your HW/Schematics based on the HW getting started in this AN: https://www.st.com/resource/en/application_note/an4938-getting-started-with-stm32h74xig-and-stm32h75xig-mcu-hardware-development-stmicroelectronics.pdf

Check mainly the power part and VCAP pins.

2 replies

mƎALLEm
Technical Moderator
October 9, 2024

Hello @sazzad07 and welcome to the community,

As you are using stm32H755 , be sure your power config is correct SMPS versus LDO which should be inline with your hardware.

What board are you using: custom or ST board?

PS: when sharing a code please use </> button.

Thank you.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
sazzad07Author
Associate
October 9, 2024

Hello @mƎALLEm  Thank you, I am using custom board with LDO as supply.I used Power Regulator Voltage Scale 0.

mƎALLEm
Technical Moderator
October 9, 2024

Hello @sazzad07 ,

Did you mistakenly mark my comment as solution?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
sazzad07Author
Associate
October 9, 2024

yes