Skip to main content
TLeaf
Associate
May 27, 2019
Question

How to configure STM32CubeIDE to support C++ development?

  • May 27, 2019
  • 26 replies
  • 40319 views

1. How to configure the IDE to use g++ compiler to compile all the files includes "*.c" files in the project?

Current it compiles the .c files by using gcc and .cpp by using g++ ...

2. If I rename main.c to main.cpp, the cube code generator will create a new main.c file instead of using main.cpp. Any sulotions for this?

Becasue main.c is .c file, so the IDE use gcc to compile this file, and this caused that I can't use any objects in it. But if I changed the main.c to main.cpp, the cube can't generate code into it...:face_screaming_in_fear:

26 replies

Harvey White
Senior III
March 18, 2021

CubeMX (any variety) creates ONLY C code.

Adding a C++ nature to a project does not change any code at all. What it does is (when going to properties/build tools) add a section where you can configure the C++ compiler.

The C++ compiler works on .hpp and .cpp files, the C compiler wants to see .c and .h. Each compiler has separate configuration sections and separate paths.

Avoid changing main.c to main.cpp; the CUBEMX tools will not update main.cpp. The solution I use gets around that problem.

Oh, and a note: the do while loop in main.c does get executed, so the code with the delay(10000) is exactly what you want if you're not using that loop.

Zacpod
Visitor II
November 4, 2021

I've just been renaming main.cpp back to main.c any time I want to change the ioc. I rename back to main.c, let it generate it's code, then rename back to .cpp so things compile properly.

It's a bit of a pain, but it's what works for me.

Harvey White
Senior III
November 4, 2021

I have forgotten to rename the .cpp to .c every now and then. Using the idea of a linking program lets you keep the .c file, and no renaming is needed. I opted for a permanent solution rather than "remember to do this each time."

AKana.1
Visitor II
June 9, 2021

hmm...

why not use standard c/c++ assotiation?

1) add new my_main.hpp:

#ifdef __cplusplus

extern "C"{

#endif

void my_cpp_main(void);

#ifdef __cplusplus

}

#endif

2) add new my_main.cpp:

#include <my_main.hpp>

void my_cpp_main(void){

// YOUR C++ "MAIN" CODE

for(;;);

}

3) add into generated main.c your header and function call:

...

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

#include "my_main.hpp"

/* USER CODE END Includes */

...

int main(void){

...

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

my_cpp_main(); /// <<<<<<<<<<<<<<<<< your c++ Infinite loop

// while (1)

 {

  /* USER CODE END WHILE */

ddelt.1
Associate
August 14, 2022

0693W00000QNe1dQAD.png 

Il est possible de renommer le fichier main.c en main.cpp et de convertir ensuite le projet en C++.

Ensuite, il faut prendre le soin d'ajouter extern "C" juste après l'insertion des directives de préprocesseur #include afin de prendre en compte le langage C dans le fichier main.cpp

Le compilateur gcc compilera les fichiers d'extension .c et g++ compilera séparément les fichiers d'extension .cpp

J'espère que ce post résoudra le problème de nombre de programmeurs.

Cordiales salutations,

Dom

ddelt.1
Associate
August 14, 2022

Voici les principaux sources de mon projet C++

Cordiales salutations,

Dom

MSZ1
Associate
August 16, 2022

Sorry for this necromancy, but this is simple problem I think.

A.h must be understandable for both C and C++ compilers.

In example below, Serial.h is C++ header with some classes and so on. A.h is included in main.c and both setup() and loop() functions are called in main.c.

A.h:

#ifndef INC_A_H_
#define INC_A_H_
 
// C INCLUDES
#include "main.h"
 
#ifdef __cplusplus
extern "C" {
 
// CPP INCLUDES
#include "Serial.h"
 
#endif
 
// DECLARATIONS
void setup();
void loop();
 
#ifdef __cplusplus
}
#endif
 
#endif /* INC_A_H_ */

A.cpp:

#include "A.h"
 
class CustomType {
 
};
 
void setup() {
 
}
 
void loop() {
 
}

XR.1
Senior
May 11, 2025

STMCubeIDE cannot handle directly C++ projects in 2025, so they will always must start with the main.c file as the entry point, no matter whether you've created a C++ project or you've converted a C project into a C++ one, as you were said before.

 

What I always do (all my projects are C++ based) is to use the main.c file as trampolin to a MainApp.cpp file (and function) so that all magic starts there.

 

In the header of the main.c file write:

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

#include "MainApp.hpp"

/* USER CODE END Includes */

 

After the initialization code you call the MainApp() function (Line 11):

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_RTC_Init();
 MX_USART2_UART_Init();
 MX_CRC_Init();
 MX_SPI1_Init();
 MX_TIM6_Init();
 MX_USART3_UART_Init();
 /* USER CODE BEGIN 2 */

 MainApp();

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */

 

You will need a MainApp.hpp file with this code:

#ifndef INC_MAINAPP_HPP_
#define INC_MAINAPP_HPP_

#ifdef __cplusplus
extern "C" {
#endif

void MainApp();

#ifdef __cplusplus
}
#endif

#endif /* INC_MAINAPP_HPP_ */

 

Finally the MainApp.cpp file with your C++ code:

// System headers for the hardware you're going to use:
#include "main.h"
#include "crc.h"
#include "rtc.h"
#include "spi.h"
#include "usart.h"
#include "gpio.h"
#include "tim.h"

// Trampolin file:
#include "MainApp.hpp"


void MainApp()
{
 while( 1 )
 {
 // whatever you want in here...
 }
}

 

IMPORTANT: The MainApp.hpp file is located inside the Inc/ folder, whilst MainApp.cpp is located into the Src/ folder.

 

Hope it helps in 2025.

 

Harvey White
Senior III
May 11, 2025

I see how this works.  (the XMEGA code generated by the old AVR studio used a trampoline to be able to deal with extended memory).

How do you deal with frequent changes to the project in CubeMXIDE?  It seems that you are copying the autogenerated setups and calls into your C++ routine.  CubeMX always generates the setups based on it's interactive settings, but (of course) only as main.c.  I picked a separate trampoline file that the main loop calls (always using FreeRTOS since the programs I write are complex enough to need it).  That way, the changes due to CubeMX are always reflected.

As an evolutionary note:

the CPP_LINK file calls my drivers for SPI, Serial, and I2C based on a board.h configuration file.  My drivers are in C++, calling the hal level drivers.  Mine wrap the hal drivers in semaphores, and allow blocking, interrupt, queue, and DMA access.  So setting up low level drivers happens here.

The CPP_LINK also sets up the main task, The main task sets up system level drivers, which are intended to be the main interface to all hardware and subsystems.  System interfaces don't care where the hardware is as long as there's a communications link to the other (or same) processor. 

Of course, this would be a lot easier if CubeMXIDE would simply recognize a main.cpp and main.h (or .hpp) file and modify it.  If no such file exists, then simply generate the main.c file as normal.  Keeps you from having to rename the main.c to main.cpp.

 

 

 

XR.1
Senior
May 13, 2025

How do you deal with frequent changes to the project in CubeMXIDE?  It seems that you are copying the autogenerated setups and calls into your C++ routine.  CubeMX always generates the setups based on it's interactive settings, but (of course) only as main.c.  I picked a separate trampoline file that the main loop calls (always using FreeRTOS since the programs I write are complex enough to need it).  That way, the changes due to CubeMX are always reflected.

 

I'm not pretty sure if I understand the question, but as long as you put your code in between the IDE "safe" placeholders, changes made to the setup code (in the STM32CubeIDE) aren't lost, like in:

 /* USER CODE BEGIN 2 */

 MainApp();

 /* USER CODE END 2 */

Doing so you don't need to write the trampoline code (and the associated code) every time.

 

BTW: A ST employee, in this very forum, told me about that the main.c file is going to be always needed.