How to replace the USC network in the Dual-mode application for STEVAL-STWINBX1
Hi,
I’m developing a voice-control system on ST’s STEVAL-STWINBX1 evaluation board. I’d like to build on the original “Dual-mode application with STM32Cube.AI and NanoEdge™ AI” by replacing the anomaly-detection function with a binary classifier based on IMP23ABSU microphone data (“xiaobei” vs. “other”). I also plan to replace the original USC model with a 10-class classification model trained on IMP23ABSU microphone data. The intended behavior is: when the MCU recognizes “xiaobei,” it should wake the USC model; otherwise, it should not.
My NanoEdge™ AI binary model is already running—when I execute start neai_class, I can see the classification output. However, after “xiaobei” is detected, the USC model fails to wake up and the firmware even falls into HardFault_Handler in some cases. I’m not sure what’s going wrong. Could you please share suggestions? For example, after modifying the USC model parameters, which source files need to be updated so the new model is compatible with the original code? Thank you!
zefang