Question
How to solve "Break at address "0xnnnnnnnn" with no debug information..."?
Hi guys
My software compiles fine. But if I try to run or debug it, it ends up with this message:
Break at address "0xf3af4804" with no debug information available, or outside of program code.
The console output is this:
STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
Log output file: C:\Users\Oli\AppData\Local\Temp\STM32CubeProgrammer_a32392.log
ST-LINK SN : 48FF6B064886575306321587
ST-LINK FW : V2J45S7
Board : --
Voltage : 3.34V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x438
Revision ID : Rev Z
Device name : STM32F303x4-x6-x8/F328xx/F334xx
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x50
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a32392.srec
File : ST-LINK_GDB_server_a32392.srec
Size : 96.00 B
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.101
Verifying ...
Download verified successfully
Shutting down...
Exit.
Does anyone have an idea how to solve this? I'm just out of any ideas.