Import CubeIDE FW Example into workspace folder
Hello All
I'm working in STMCubeIDE 2.0.0 Windows.
I have downloaded STM32Cube_FW_F4_V1.28.0 package and saved it here: C:\Users\marin\STM32Cube\Repository\STM32Cube_FW_F4_V1.28.0
I want to use an example and build a project from the example.
This LCD example: C:\Users\marin\STM32Cube\Repository\STM32Cube_FW_F4_V1.28.0\Projects\STM32F429I-Discovery\Applications\Display\LTDC_Paint.
I don't want to change the original example code, I want to put the example into a new folder and do my changes there.
I saw using "Copy to workspace" when importing is a mess and don't compile: No rule to make target 'C:/Middlewares/ST/STM32_USB_Host_Library/Core/Src/usbh_core.c'
Do I have to copy the whole directory to a new location? C:\Users\marin\STM32Cube\Repository\STM32Cube_FW_F4_V1.28.0\Projects\STM32F429I-Discovery\Applications\Display\LTDC_Paint.
Please show me a way to copy the example code (Only LTDC_Paint project) to a new location and successfully compile.
Marinus