Included path seems to not be included everywhere
Hi,
I am working on a preexisting TouchGFX projects, and i am trying to make it multicore so i am trying to build with OpenAMP to test if i didn't tweak wrong settings in CubeMX
I added the path in Project > Properties > C/C++ General > Preprocessor Include Paths , but when i try to build the project on CubeIDE it fails saying (the dots are to smoothen reading)
..../HMI__stm32/BENCH10/CM7/Core/Src/main.c:35:10: fatal error: openamp.h: No such file or directory
When building the first part (gcc) does include it
arm-none-eabi-gcc "C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/Common/Src/system_stm32h7xx_dualcore_boot_cm4_cm7.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DCORE_CM7 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../../../CM7/OPENAMP -I../../../CM7/Core/Inc -I../../../CM7/FATFS/Target -I../../../CM7/FATFS/App -I../../../CM7/TouchGFX/App -I../../../CM7/TouchGFX/target/generated -I../../../CM7/TouchGFX/target -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Drivers/STM32H7xx_HAL_Driver/Inc" -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Utilities/JPEG -I../../../Middlewares/Third_Party/FatFs/src -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM7/USB_HOST/App -I../../../CM7/USB_HOST/Target -I../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../CM7/../../CM7/Middlewares/ST/touchgfx/framework/include -I../../CM7/../../CM7/TouchGFX/generated/fonts/include -I../../CM7/../../CM7/TouchGFX/generated/gui_generated/include -I../../CM7/../../CM7/TouchGFX/generated/images/include -I../../CM7/../../CM7/TouchGFX/generated/texts/include -I../../CM7/../../CM7/TouchGFX/generated/videos/include -I../../CM7/../../CM7/TouchGFX/gui/include -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -include"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Application/User/Core/uart_handler.h" -Os -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/CMSIS/system_stm32h7xx_dualcore_boot_cm4_cm7.d" -MT"Drivers/CMSIS/system_stm32h7xx_dualcore_boot_cm4_cm7.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/system_stm32h7xx_dualcore_boot_cm4_cm7.o"
Then the g++ too (This is the line directly after the previous)
arm-none-eabi-g++ "C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/CM7/TouchGFX/gui/src/common/FrontendApplication.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DDEBUG -DCORE_CM7 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../../../CM7/OPENAMP -I../../../CM7/Core/Inc -I../../../CM7/FATFS/Target -I../../../CM7/FATFS/App -I../../../CM7/TouchGFX/App -I../../../CM7/TouchGFX/target/generated -I../../../CM7/TouchGFX/target -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Utilities/JPEG -I../../../Middlewares/Third_Party/FatFs/src -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM7/USB_HOST/App -I../../../CM7/USB_HOST/Target -I../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../CM7/../../CM7/Middlewares/ST/touchgfx/framework/include -I../../CM7/../../CM7/TouchGFX/generated/fonts/include -I../../CM7/../../CM7/TouchGFX/generated/gui_generated/include -I../../CM7/../../CM7/TouchGFX/generated/images/include -I../../CM7/../../CM7/TouchGFX/generated/texts/include -I../../CM7/../../CM7/TouchGFX/generated/videos/include -I../../CM7/../../CM7/TouchGFX/gui/include -I"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Application/User/Core" -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -Os -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -femit-class-debug-always -fstack-usage -MMD -MP -MF"Application/User/gui/FrontendApplication.d" -MT"Application/User/gui/FrontendApplication.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Application/User/gui/FrontendApplication.o"
But after this, evertime gcc is used, it is not
arm-none-eabi-gcc "C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/CM7/USB_HOST/Target/usbh_conf.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DCORE_CM7 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../../../CM7/Core/Inc -I"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Application/User/Core" -I../../../CM7/FATFS/Target -I../../../CM7/FATFS/App -I../../../CM7/TouchGFX/App -I../../../CM7/TouchGFX/target/generated -I../../../CM7/TouchGFX/target -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Drivers/STM32H7xx_HAL_Driver/Inc" -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Utilities/JPEG -I../../../Middlewares/Third_Party/FatFs/src -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM7/USB_HOST/App -I../../../CM7/USB_HOST/Target -I../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../CM7/../../CM7/Middlewares/ST/touchgfx/framework/include -I../../CM7/../../CM7/TouchGFX/generated/fonts/include -I../../CM7/../../CM7/TouchGFX/generated/gui_generated/include -I../../CM7/../../CM7/TouchGFX/generated/images/include -I../../CM7/../../CM7/TouchGFX/generated/texts/include -I../../CM7/../../CM7/TouchGFX/generated/videos/include -I../../CM7/../../CM7/TouchGFX/gui/include -include"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Application/User/Core/uart_handler.h" -Os -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Application/User/USB_HOST/Target/usbh_conf.d" -MT"Application/User/USB_HOST/Target/usbh_conf.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Application/User/USB_HOST/Target/usbh_conf.o"
Right after this there are instances of g++ including it
arm-none-eabi-g++ "C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/CM7/TouchGFX/target/generated/HardwareMJPEGDecoder.cpp" -mcpu=cortex-m7 -std=gnu++14 -g3 -DDEBUG -DCORE_CM7 -DUSE_HAL_DRIVER -DSTM32H757xx -c -I../../../CM7/OPENAMP -I../../../CM7/Core/Inc -I../../../CM7/FATFS/Target -I../../../CM7/FATFS/App -I../../../CM7/TouchGFX/App -I../../../CM7/TouchGFX/target/generated -I../../../CM7/TouchGFX/target -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Utilities/JPEG -I../../../Middlewares/Third_Party/FatFs/src -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM7/USB_HOST/App -I../../../CM7/USB_HOST/Target -I../../../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../../../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc -I../../CM7/../../CM7/Middlewares/ST/touchgfx/framework/include -I../../CM7/../../CM7/TouchGFX/generated/fonts/include -I../../CM7/../../CM7/TouchGFX/generated/gui_generated/include -I../../CM7/../../CM7/TouchGFX/generated/images/include -I../../CM7/../../CM7/TouchGFX/generated/texts/include -I../../CM7/../../CM7/TouchGFX/generated/videos/include -I../../CM7/../../CM7/TouchGFX/gui/include -I"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Application/User/Core" -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -Os -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -femit-class-debug-always -fstack-usage -MMD -MP -MF"Application/User/TouchGFX/target/generated/HardwareMJPEGDecoder.d" -MT"Application/User/TouchGFX/target/generated/HardwareMJPEGDecoder.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Application/User/TouchGFX/target/generated/HardwareMJPEGDecoder.o"
And the last part (gcc) doesnt:
arm-none-eabi-gcc -mcpu=cortex-m7 -g3 -DDEBUG -c -I"C:/Users/Max/Downloads/Programmes/Programmes/HMI__stm32/BENCH10/STM32CubeIDE/CM7/Application/User/Core" -I../../CM7/../../CM7/Middlewares/ST/touchgfx/framework/include -I../../CM7/../../CM7/TouchGFX/generated/fonts/include -I../../CM7/../../CM7/TouchGFX/generated/gui_generated/include -I../../CM7/../../CM7/TouchGFX/generated/images/include -I../../CM7/../../CM7/TouchGFX/generated/texts/include -I../../CM7/../../CM7/TouchGFX/generated/videos/include -I../../CM7/../../CM7/TouchGFX/gui/include -x assembler-with-cpp -MMD -MP -MF"Application/User/Startup/startup_stm32h757xihx.d" -MT"Application/User/Startup/startup_stm32h757xihx.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Application/User/Startup/startup_stm32h757xihx.o" "../Application/User/Startup/startup_stm32h757xihx.s"
What i tried so far:
I tried regenerating code with TouchGFX designer,
i tired doing so after deleting /TouchGFX/target/generated, /TouchGFX/generated and /build, regenerating with Designer, clean on IDE and rebuild.
Under GPT supervision i tried tweaking settings, perhaps i did it wrong
It is my first time working on a stm project, so i am not familiar with the settings etc