Skip to main content
Associate III
January 24, 2025
Question

ISM330DHCX - How to use X-CUBE-MEMS1 generated library with SPI?

  • January 24, 2025
  • 1 reply
  • 529 views

Hi 

"I am using the STM32F407 to interface with the ISM330DHCX. I have installed the X-CUBE MEMS1 package, configured the SPI1 protocol, and generated the code. However, I have absolutely no idea how to initialize and use the sensor in my main.c code. How should I write the code correctly?" Let me know some suggestions.

1 reply

ELABI.1
Technical Moderator
January 29, 2025

Hi @Kumar123

You can refer to this detailed article on How to integrate the X-CUBE-MEMS1 package with your project and also to this article How to install and import an X-CUBE Expansion Package with STM32CubeMX.

Thank you.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Kumar123Author
Associate III
January 30, 2025

Hi ELABI.1

"I've written the logic based on the example, but the values aren't being generated as expected."