Issue: No source available for Bootloader
Hello,
My project was working fine, but suddenly I cannot debug or run it with the original bootloader anymore. The project is created and generated by TouchGFX Designer.
This is the error message I get when I try to debug/run the project.

I am sure that the bootloader bin file is already there in the correct path and the corresponding path is also already correct in the linker script.
If I remove the bootloader part from the linker script and flash my customized bootloader from CubeProgrammer then I could run the application but as I said I need to debug the project.
Anyone have such problem before or know how to solve it?
BR,