Skip to main content
Associate
September 27, 2025
Question

MC SDK 6.4.1 is out, Congratulations!

  • September 27, 2025
  • 1 reply
  • 412 views

Have you fixed the project opening problem with CubeIDE?

You mustn't open the generated project, mustn't import the project, you only can use the button in the MX message-window, "open project". If you don't, you cannot compile the project.

After that, new errors are coming: PDSC version is not supported. There is no "PDSC settings" in the projekt, so what is it?

These applications (CubeIDE + MX + MC SDK) are still unstable and very slow products!

1 reply

Associate II
September 27, 2025

Where did you get 6.4.0 from?

 

They gave me only Cube IDE 1.19.0 :(

This seems to work better ...

FT1Author
Associate
September 27, 2025

Hi mfgkw,


I am afraid that I mistyped the version number earlier (MC SDK 6.4.0).

Versions that I tried out:

IDE: 1.19.0.

MX: 6.13., 6.15.,

MCSDK: 6.3.2., 6.4.1.


In each case I experienced that I wrote.

Moreover these applications create a lot of garbage on my SSD. This garbage remained even after uninstalling, so before I reinstall them, I tried to clear a lot of file in the C:/users/myname/.STMCube, .../.STM32CubeIDE, .../.ST_Workbench, .../STM32CubeMX, .../STCubeIDE.

So regardless of version numbers I am saying it is an unstable, and slow software ecosystem.

I have no idea how they can validate these things. 


Best Regards,

FT1